SLLA486B May 2020 – October 2024 ISO1042 , ISO1042-Q1 , ISO1044 , ISO1050 , ISOW1044
CANH to GND or CANL to GND capacitance will eventually end up as differential capacitance across CAN bus.
Isolated CAN data sheet gives rise/fall times with 100 pF bus capacitance, but if differential capacitance is increased, driver rise and fall times will slow down eating up the timing budget. Various components will contribute to this capacitance:
Recessive to dominant edge will depend on the driver to charge up this differential bus capacitance. Usually this process will be faster given an active current source is charging up this capacitance. On dominant to recessive edge, driver is turned off, so this transition will happen due to RC decay of the network. Here R is the effective differential resistance, say 60 ohm (two terminations in parallel). C is the effective differential capacitance of the network (which is the sum of all 4 components that were stated above as all are in parallel).
Say L is total cable length in meter, N is number of nodes each offering CID differential capacitance per selected ISOCAN data sheet (ignoring external CMC / TVS, and connector capacitance just for simplicity here):
Entering values in Equation 2.
From previous equation, maximum bus capacitance that can be introduced across the bus, Cmax can be calculated. CANH to GND and CANL to GND can be double this value. This is the theoretical maximum. Components ignored will also impact. Our recommendation to the customer is to thoroughly test for any bit errors in their system.