SLUA887A August 2018 – September 2023 UCC27201A , UCC27710 , UCC27712 , UCC27714
This time constant occuring during the high-side off time explains the dependency on duty cycle. This duty cycle being constant, the bootstrap resistor and bootstrap capacitor should be tuned appropriately to achieve the desired start-up time. Increasing the bootstrap resistor values will increase the time constant leading to slower start-up time.
Additionally, the bootstrap resistor chosen must be able to withstand high power dissipation during the first charging sequence of the bootstrap capacitor. This energy can be estimated by Equation 7:
This energy is dissipated during the charging time of the bootstrap capacitor and can be estimated using Equation 8:
This resistor is essential in limiting the peak currents through the bootstrap diode at start-up and limiting the dv/dt of HB-HS (high-side floating supply to the return high-side floating supply). The peak current through this resistor can be calculated using Equation 9:
Figure 3-4 shows the fast ramp up on VDD (CH4) and HB-HS (CH1) when using a 0-Ohm resistor which leads to undesired change in voltage on LO(CH3) and HO(CH2).
Figure 3-5 shows how using slightly higher resistor value (Rboot = 2.2Ohms) solve this issue. It is important to note that the bias rising rate observed in Figure 3-5 does not apply to all drivers.