SLVAFD4 February 2024 TPS54308 , TPS54320 , TPS54350 , TPS54620 , TPS54622 , TPS54821 , TPS54824 , TPS62933F
The experimental validation is completed with PCM converter TPS62933F. Operating condition is: Vin=24V, Vout=1.2V, fsw=500kHz, Iout=0A. Required output voltage ripple amplitude is smaller than 800uV pk-pk.
As comparison, an application case without second stage filter is given at first. With typical recommended components value in data sheet, L=2.2 uH and Co=94uF are selected for this operating condition. 2 x 47uF capacitors are used for the 94uF Co.
The output voltage ripple test waveform is shown as Figure 3-1, the output voltage ripple pk-pk amplitude is about 5.7mV and it is much larger than the requirement.
Then the proposed components selection method of second stage filter is verified. With same 2 x 47uF as the total capacitance for both first stage and second stage filters, we set the Co=1x47uF and C2=1 x 47uF. Substituting all parameters into Equation 7, L2≥14.9nH could be got as the restriction for 800uV output voltage ripple.
Select L2=20nH and Figure 3-2 shows the output voltage ripple with second stage filter. The output voltage ripple amplitude is 640uV pk-pk and could satisfy the 800uV requirement.
The effectiveness of proposed design method is verified by the example. More experimental results are shown in Section 7.