SNLA461 July 2024 DS320PR1601 , DS320PR410 , DS320PR810 , SN75LVPE5412 , SN75LVPE5421
PCIe linear redrivers are designed to compensate for signal distortion caused by insertion loss from traces and other elements in the path of a PCIe signal. This is done through special CTLE amplifiers that boost the high-frequency content of incoming signals. This process of equalization, or EQ, is one of the fundamental tools of PCIe signal conditioning across different product categories. While simpler at a theoretical level than the additional digital processing capabilities offered by PCIe retimer, the analog properties of equalization already have complexities that can be confusing to engineers who are new to the field of signal integrity. This application note can explain the background and operation of PCIe redriver equalization in an intuitive and detailed way to assist engineers in planning and using TI PCIe redrivers in designs.
All trademarks are the property of their respective owners.
PCIe, or Peripheral Component Interconnect Express, is a high-speed data transfer standard commonly used in computers and enterprise systems to interface between CPUs and various types of endpoints such as GPUs and SSDs. It is also attracting interest in new areas such as automotive applications. PCIe is an ubiquitous protocol with many advantages: it uses a simple NRZ (non-return-to-zero) differential signaling scheme and the structure based on multiple individual lanes allows it to support both small and large applications as needed.
Industry trends have led to greater and greater PCIe data rate demands with successive generations. PCIe Gen 1 from 2003 allowed for 2.5 GT/s of data transfer per lane. PCIe Gen 5 from 2017 provides for up to 32 GT/s, an increase of nearly 13x. No modifications were made to the original NRZ signaling scheme from Gen 1 to Gen 5 and such data rate increases were accomplished by increasing the symbol rate, leading to new challenges in signal integrity. Signal conditioning devices such as redrivers and retimers are designed to address these problems by maintaining signal quality over higher data rates and longer reaches. Though many methods can be used to condition signals, equalization is one of the most fundamental and is intimately tied to the properties of the materials that signals propagate through.