SNLA473 November 2024 DP83867CS , DP83867E , DP83867IS , DP83869HM , DP83TC811S-Q1 , DP83TC812S-Q1 , DP83TC813S-Q1 , DP83TC814S-Q1 , DP83TC817S-Q1 , DP83TC818S-Q1 , DP83TG720S-Q1 , DP83TG721S-Q1
Before proceeding with any further debug, check that the PHY being used has been correctly strapped into SGMII mode by checking the Strap Configuration section of the data sheet.
The strap status of the PHY can be confirmed by reading the CHIP_SOR or SOR_VECTOR register (depending on device).These registers can be accessed using extended register access.
Figure 1-1 is an example of SGMII strap configurations for the DP83TG720S-Q1 Automotive Ethernet PHY. The default MAC Interface of the DP83TG720S-Q1 is SGMII so pins RX_D0, RX_D1, and RX_D2 can be left floating.