SPRACY9 March   2023 F29H850TU , F29H850TU , F29H859TU-Q1 , F29H859TU-Q1 , TMS320F2800132 , TMS320F2800132 , TMS320F2800133 , TMS320F2800133 , TMS320F2800135 , TMS320F2800135 , TMS320F2800137 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280023C , TMS320F280025 , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280033 , TMS320F280034 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C , TMS320F280049C-Q1 , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28076 , TMS320F28374D , TMS320F28374D , TMS320F28374S , TMS320F28374S , TMS320F28375D , TMS320F28375D , TMS320F28375S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376D , TMS320F28376S , TMS320F28376S , TMS320F28377D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378D , TMS320F28378S , TMS320F28378S , TMS320F28379D , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28379S , TMS320F28384D , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388D , TMS320F28388S , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1 , TMS320F28P659SH-Q1

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Mechanism of ADC Input Settling
    2. 1.2 Symptoms of Inadequate Settling
      1. 1.2.1 Distortion
      2. 1.2.2 Memory Cross-Talk
      3. 1.2.3 Accuracy
      4. 1.2.4 C2000 ADC Architecture
    3. 1.3 Resources
      1. 1.3.1 TINA-TI SPICE-Based Analog Simulation Program
      2. 1.3.2 PSPICE for TI Design and Simulation Tool
      3. 1.3.3 TI Precision Labs - SAR ADC Input Driver Design Series
      4. 1.3.4 Analog Engineer's Calculator
      5. 1.3.5 Related Application Reports
      6. 1.3.6 PSpice for TI ADC Input Models
  4. 2Input Settling Design Steps
    1. 2.1 Select the ADC
    2. 2.2 Find the Minimum Op-Amp Bandwidth and RC Filter Ranges
      1. 2.2.1 Select Type
      2. 2.2.2 Resolution
      3. 2.2.3 Csh
      4. 2.2.4 Full-Scale Range
      5. 2.2.5 Acquisition Time
      6. 2.2.6 Outputs
      7. 2.2.7 Math Behind the Calculator
    3. 2.3 Select an Op-Amp
    4. 2.4 Verify the Op-Amp Model
    5. 2.5 Build the ADC Input Model
      1. 2.5.1 Vin
      2. 2.5.2 Voa, Voa_SS, and Verror
      3. 2.5.3 Rs, Cs, and Vcont
      4. 2.5.4 Ch, Ron, and Cp
      5. 2.5.5 S+H Switch, Discharge Switch, tacq, and tdis
    6. 2.6 Refine RC Filter Values Via Simulation
    7. 2.7 Perform Final Simulations
    8. 2.8 Input Design Worksheet
  5. 3Example Circuit Design
    1. 3.1  Select the ADC
    2. 3.2  Find the Minimum Op-Amp Bandwidth and RC Filter Ranges
    3. 3.3  Verify the Op-Amp Model
    4. 3.4  Build the ADC Input Model
    5. 3.5  Bias Point Analysis to Determine Voa_ss
    6. 3.6  Transient Analysis to Determine Voa_ss
    7. 3.7  Perform Initial Transient Analysis
    8. 3.8  Iterative Approach to Refine RC Filter Values
    9. 3.9  Perform Final Transient Analysis
    10. 3.10 Perform Final Transient Analysis
    11. 3.11 Further Refinement
    12. 3.12 Further Simulations
    13. 3.13 Completed Worksheet
  6. 4Working With Existing Circuits or Additional Constraints
    1. 4.1 Existing Circuits
      1. 4.1.1 Brief Overview of Charge Sharing
      2. 4.1.2 Charge Sharing Example
      3. 4.1.3 Additional Resources for Charge Sharing
    2. 4.2 Pre-Selected Op-Amp
      1. 4.2.1 Pre-Selected Op-Amp Example
    3. 4.3 Pre-Selected Rs and Cs Values
      1. 4.3.1 Analytical Solution for ADC Acquisition Time
      2. 4.3.2 Example Analytical Solution for ADC Acquisition Time
  7. 5Summary
  8. 6References

Further Refinement

Overall, it appears that this design has quite a bit of settling margin. If further optimization is desired, the designer could explore using an op-amp with slightly lower bandwidth. Alternatively, the simulation supports using a S+H window that is shorter than 100 ns, if desired.

Another area refinement is to resolve a circuit with intentionally higher Rs and Cs. As designed, the low-pass filter bandwidth of the Rs and Cs circuit is about 15 MHz, so this circuit provides some rejection of high-frequency noise. By intentionally increasing Rs and Cs, the filter bandwidth can be lowered, resulting in additional noise rejection. However, note that the Rs and Cs circuit can generally not provide a true anti-aliasing filter, as this would necessarily result in a settling time constant that would be much too large to allow proper settling. If a true anti-aliasing filter is needed, this should be built as a separate filter stage before the ADC drive stage.

CAUTION: Even if the simulations indicate that the input could settle faster than the minimum acquisition window specified in the device-specific data manual, do not select an acquisition window that violates the device-specific data manual minimum acquisition window time.