SPRAD12A July 2022 – February 2023 F29H850TU , F29H859TU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
To begin, the positive duty of the dead-band is verified. The desired frequency is 400 kHz for EPWM1, EPWM2, and EPWM3. As seen in GUID-63979800-A180-4E36-A63C-DF48DD878B3D.html#GUID-D19DF68A-A5E6-4FDB-BC79-4460E5820DBC the period of the ePWM outputs should be 2.5 µsec. Based on GUID-63979800-A180-4E36-A63C-DF48DD878B3D.html#GUID-29E50045-301A-44BB-AEA3-7DF4C8552950, the TBPRD value is 125, meaning the time-base counter of the ePWM module counts from 0 to 125 and then back down to 0, since the counter mode is set to up-down. This yields a total of 250 counts over one period. Therefore, each count of the time-base counter is 10 nsec based on #GUID-51930023-77FF-45BA-A4DF-1BDE69E7A9FB.
The counter compare values are set at 69. For the A output, when the time-base counter equals the counter compare while it is counting up, the output is set to go high. When the time-base counter is counting down and there is a match with the counter compare value, then the output is supposed to go low. However, the dead-band submodule has also been set up to incorporate dead-time in the output. As seen through GUID-B8AD9A13-19AA-4EAA-92F9-01A70D8A12F0.html#GUID-E3B6BF83-A17E-46D5-93A1-51EEE273148A, the DBRED and DBFED are set to 20 in order to have a dead-time of 200 nsec, shown in #GUID-10D9A881-1809-4DE9-9B87-7650541787EC. Therefore, for EPWMxA, the output does not go high when the time-base counter equals 69 (CMPA value), but rather 89 since there are 20 counts of dead-time inserted for the rising edge. #GUID-4B1F6A2F-D03B-4E38-A540-1311E7D63F7F shows how to calculate the duty cycle based on this information.
Putting it in terms of time, 92 * 10 nsec is 920 nsec, so the positive pulse width should be 920 nsec as seen in #GUID-1B838787-5392-461B-B64C-807A832CB5B7.