SPRADG6 April 2024 F28M36H33B2 , F29H850TU , F29H859TU-Q1 , SM320LF2407A-EP , TMS320C28341 , TMS320C28343 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28035-EP , TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052M-Q1 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28062F-Q1 , TMS320F28064 , TMS320F28066-Q1 , TMS320F28068M , TMS320F28069F-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F2810 , TMS320F2811 , TMS320F28333 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SJ , TMS320F28P559SJ-Q1 , TMS320F28P650DK , TMS320F28P659DK-Q1
With Discrete solution, make sure to have following criteria met to ensure ASIL-B requirement.
This is one of the important steps when we want to design a power supply and monitoring solution for the MCU and the rest of the system. Calculate the maximum current consumption value of IDD and IDDIO for MCU from its data sheet and include all the current consumption of other components on each rail.
As for electrical noise, LDOs can reach a lower noise floor than buck converters. This is because buck converters (and other switching power supplies) use inductors that have the tendency to produce significant noise.
Select an IC that can monitor VDD and VDDIO Supply rails. Use either the single Multichannel Supervisor or separate supervisor for each of the power rails. Select ICs that are functional safety complaint and auto qualified. For the monitoring of VDD, see the device-specific data sheet.
Make sure IC selected is functional safety capable and auto qualified.
VREF can be supplied externally or internally. Using the internal reference for the ADC provides better accuracy compared to an external reference using a supply rail. If external VREF is used, use the buffer to minimize the noise on the rail. Based on the functional safety goals of the application, voltage monitoring of ADC VREF may be required.
You can use an external watchdog or supervisor with integrated window/Q&A watchdog.