SWRA513C January 2020 – September 2020 CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Once a new profile is configured to the device, it must be confirmed. A profile is successfully confirmed only if: the WLAN connection was successful, an IP address was successfully acquired, and the user’s smartphone provisioning app (that configured the profile) received the successful confirmation result from the device (feedback). After a successful confirmation, the device can either stay connected to the new network (STA role), or switch back to the AP role.