SPRACZ7 January 2022 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28232 , TMS320F28232-Q1 , TMS320F28234 , TMS320F28234-Q1 , TMS320F28235 , TMS320F28235-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
C2000 is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.
The TMS320F2833x/2823x and TMS320F2837xD/2837xS/2807x are device members of the C2000 MCU product family. These devices are most commonly used in embedded control applications. The TMS320F2837xD/2837xS/2807x devices feature an updated version of the enhanced control peripherals found on the TMS320F2833x/2823x, which allows for greater flexibility and improved application performance. In addition, the TMS320F2837xD/2837xS/2807x devices feature a boot mode flow which enables expanded booting options that provide the ability to use alternate boot mode selection pins. Enhancements to the CPU include the addition of a trigonometric math unit (TMU) and a Viterbi/Complex Math Unit (VCU-II). Other device enhancements include eight cross-bars (XBARs) for providing a flexible means for interconnecting multiple inputs, outputs, and internal resources.
For the purposes of migration, these devices will be referenced in two groups:
For a full list of devices currently available within the F2833x/23x and F2837xD/S/07x families, see the TI website at http://www.ti.com/c2000.
As the focus of this document is to describe the differences between the two device groups, the descriptions are explained only to the extent of highlighting areas that require attention when moving an application from one device to the other. For a detailed description of features specific to each device, see the device-specific technical reference manuals available on the TI website. This application report does not cover the silicon exceptions or advisories that may be present on each device.
Consult the following silicon errata for specific advisories and workarounds:
The following abbreviations are used in this document: