SBAA535A March 2022 – March 2024 ADC128D818 , ADS1000 , ADS1000-Q1 , ADS1013 , ADS1013-Q1 , ADS1014 , ADS1014-Q1 , ADS1015 , ADS1015-Q1 , ADS1018 , ADS1018-Q1 , ADS1100 , ADS1110 , ADS1112 , ADS1113 , ADS1113-Q1 , ADS1114 , ADS1114-Q1 , ADS1115 , ADS1115-Q1 , ADS1118 , ADS1118-Q1 , ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS1146 , ADS1147 , ADS1148 , ADS1148-Q1 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1216 , ADS1217 , ADS1218 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS1243-HT , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS1281 , ADS1282 , ADS1282-SP , ADS1283 , ADS1284 , ADS1287 , ADS1291 , LMP90080-Q1 , LMP90100 , TLA2021 , TLA2022 , TLA2024
Table 8-8 reports the system parameters that determine the cycle time in Example #1:
PARAMETER | VALUE |
---|---|
ADC | ADS124S08 |
ODR | 1000 SPS |
Filter type | sinc3 |
Clock frequency | 4.096 MHz (default) |
Conversion mode | Continuous |
Programmable delay | 14 ∙ tMOD (default) |
Chopping | Disabled |
Conversions per channel | 3 |
# of channels | 2 |
First, this example uses the default clock frequency, fCLK, of 4.096 MHz, allowing the nominal conversion latency values reported in the data sheet to be used. Next, it is necessary to consider both first conversion versus second and subsequent conversion latency for this example because there are multiple conversions required per channel and continuous-conversion mode is used.
Reviewing Table 5-1, the ADS124S08 conversion latency using the sinc3 filter and ODR = 1000 SPS is 3.156 ms for first conversion data (tFC) and 1 ms for second and subsequent conversions (tSSC). These times include the ADC overhead but do not include the programmable delay, tDELAY, where applicable. Equation 14 calculates the value of tDELAY in microseconds using the default value of tDELAY = 14 ∙ tMOD and fCLK = 4.096 MHz:
The ADS124S08 programmable delay does not affect tSSC, though it does affect tFC. The first conversion latency including programmable delay, tFC_TOTAL, is calculated by Equation 7:
Finally, there is no need to consider additional latency due to chopping. Since each channel includes one first conversion and two second or subsequent conversions, the scan time for one channel, tCH, is given by Equation 8:
Equation 9 calculates the cycle time, tCYCLE, using the result from Equation 8:
Ultimately, the cycle time for this example is 10.422 ms for 6 conversion results. Figure 8-1 depicts a timing diagram for the example system given the design parameters.