SBAU428 September   2023 AFE7728D , AFE7768D , AFE7769 , AFE7769D , AFE7799 , AFE7920 , AFE7921 , AFE7952 , AFE7988 , AFE7989 , AFE8030 , AFE8092

 

  1.   Abstract
  2.   2
  3.   Trademarks
  4. 1Introduction
  5. 2Hardware Setup
  6. 3Software Setup
  7. 4Bring-Up Steps
  8. 5TX to FB Loopback With DDR Example
  9.   A Setting Ethernet Port IP Address

Bring-Up Steps

The following section provides a step-by-step walkthrough of the reference design setup from a bring-up perspective, along with relevant screenshots of the process throughout.

Steps:

  1. First, power on the Agilex eSOM7 TI Carrier and then power on the TI AFE7769DEVM.
  2. Open Teraterm, click on "Serial", and click "OK".
  3. Click on Setup > Serial port, see Figure 4-1.
    GUID-20230703-SS0I-5B4S-1PXF-SKC0S3CJ7CMN-low.png Figure 4-1 Opening Serial Port Window in Teraterm
  4. A new window will appear. Select the COM port that the eSOM7 is connected to (not COM1). Change the speed to 115200 and click "Close and New open", see Figure 4-2.
    GUID-20230703-SS0I-KV8P-1PKK-5KHQ7BJDN3GF-low.png Figure 4-2 Serial Port Setup and Connection
  5. You should now see "agilex login:", if you do not see any text, hit enter and "agilex login" will appear.
  6. Type root and hit enter to login.
  7. Get the IP address of the Arm node using the ifconfig command. If you do not see an "inet4" IP address under the eth0 interface, use the command ifconfig eth0 192.168.0.1 netmask 255.255.255.0 to assign the 192.168.0.1 IP address to the eth0 interface, see Figure 4-3.
    GUID-20230703-SS0I-SSKH-5P17-DWKXKSD62C2C-low.png Figure 4-3 IP Address Acquisition
  8. On PowerShell, move your directory to the Hitek RF INTF release archive using the cd < Hitek RF INTF release archive path> command. In our setup, the command was cd C:\Users\a0503061\Documents\Hitek\AG_eSOM_AFE77XX_RF_INTF_DEMO_Release_v3_3_2023-04-2 5.
  9. Copy the software/arm_ag_/tools folder from the AG_eSOM_AFE77XX_RF_INTF_DEMO_Release_v3_3_2023-04-25 folder to the Arm node with the folder name as jesd_tools using the command scp -r software/arm_ag/tools/ root@192.168.0.1:~/jesd_tools/.
  10. Start the TI AFE77xxD Latte GUI software and in the first dialog window titled "Latte Mode", make sure that FPGA_Type is set to "None" and the "AFE EVM Card Detected" message appears. The message "Couldn't Detect FPGA Reset FTDI. Reset FPGA manually." is expected. Then press "Continue" button to open the main Latte GUI. For proper navigation to Latte mode window, see Figure 4-4.
    GUID-20230703-SS0I-3ZCX-2WN1-4SKXCLMS99PC-low.png Figure 4-4 Launching the AFE77xxD Latte GUI
  11. After the Latte software goes through its initialization steps, go to the AFE77xxD Params tab by clicking on AFE77xxD-Params on the left panel of the software window. Figure 4-5 shows how to navigate to the respective tab on the software panel.
    GUID-20230703-SS0I-TWDJ-MZ0B-V8GG6TNFBSLG-low.png Figure 4-5 Navigating to AFE77xxD-Params
  12. In the "Load System Parameters" box, click the "Browse" to search for the AFE77xxD_Config.json config file provided in AG_eSOM_AFE77XX_RF_INTF_DEMO_Release_v3_3_2023-04-25\software\x64_64\utilities\AFE77xxDLatte_v0p4 and open it. For a view of the "AFE77xxD-Params" display and how to load the file, see Figure 4-6 and Figure 4-7, respectively.
    GUID-20230703-SS0I-CJJH-ZNLX-F6LQPBD63B7R-low.png Figure 4-6 View of the AFE77xxD-Params Display
    GUID-20230703-SS0I-C0WZ-75JS-P1BPS3BVCJFV-low.png Figure 4-7 Loading the AFE77xxD Configuration File Into Latte
  13. After selecting the configuration file, please click the "LOAD" button to load the configuration into the GUI. The GUI should change to the required configuration to be able to perform JESD link up with the JESD IP in the Agilex FPGA.
  14. Open Quartus Prime Programmer and click the "Auto Detect" button. For navigation to the respective function, see Figure 4-8. If this is the first time the eSOM7 is connected to the PC and the "Auto Detect" button is grayed out, click on the "Hardware Setup..." button, select the "HTK USBII" in the drop down next to "Currently selected hardware" and check that the "Hardware frequency" is set to 24000000Hz.
    GUID-20230703-SS0I-9B8R-B8LB-WWXMQSPFMD82-low.png Figure 4-8 Auto Detect in Quartus Prime Programmer
  15. After clicking "Auto Detect", a window will appear; select the AGFB027R24CR2 option and click "OK". Figure 4-9 shows the typical view when selecting a device.
    GUID-20230703-SS0I-GBVF-ZPHF-3VVBH0BNGRHZ-low.png Figure 4-9 Device Selection
  16. Select the only row under "File" and then click on “Change File”. Select the FPGA image called ag_esom_top_afe77xx_jesd204c_4t4r2f_fpga_first_hps_auto.sof that is provided in the directory AG_eSOM_AFE77XX_RF_INTF_DEMO_Release_v3_3_2023-04-25\snapshots\hardware\fpga\agfb027_r24c_asyXX\ag_esom_top_afe77xx_jesd204c_4t4r2f_fpga_first_20230421_012455, where "XX" should match the "ASY-XX-00047" label on the eSOM7 board. There is an extra copy of these files in a compressed .tar.gz folder. Figure 4-10 shows how to navigate to the proper functions.
    GUID-20230703-SS0I-F2C9-MKMT-L47MMMPRB6G3-low.png Figure 4-10 File Change
  17. Next, check the box under "Program/Configure", see Figure 4-11.
    GUID-20230703-SS0I-7WWV-HQZ9-SZN7JZL6SQJG-low.png Figure 4-11 Program/Configure
  18. On the AFE77xxD GUI, the “Device Bringup” button at the bottom of the AFE77xxD-Params page should be clicked to start the configuration of the LMK04828 and AFE7769D chips. Figure 4-12 shows how to navigate to the respective button.
    GUID-20230703-SS0I-5KDG-BS6X-HHCGDQ1DRSB9-low.png Figure 4-12 Device Bringup, AFE77xxD-Params
  19. Once the “LMK Configured” message appears in the TI AFE77xxD Latte software log window indicating completion of the LMK04828 chip configuration, program the Agilex FPGA image by clicking the “Start” button on Quartus Prime Programmer. Figure 4-13 and Figure 4-14 show a visual reference of the steps to program the device.
    GUID-20230703-SS0I-FNQP-NKSK-FXGCSX81TFZZ-low.png Figure 4-13 Confirmation of LMK Configuration in the AFE77xxD Latte GUI
    GUID-20230703-SS0I-RLK5-VBW7-RVGWSJ02ZFXR-low.png Figure 4-14 Clicking the Start Button to Program the Agilex FPGA
  20. Wait for Linux bootup of the Arm node to show up on the Teraterm console and login with the root username. Then, use the command source jesd_tools/init_term.sh to execute the init_term.sh script in the jesd_tools folder, and run the run_jesd_init_afe77xx_jesd204c_4t4r2f_board.sh script on the Arm node. Do not hit enter yet. Figure 4-15 shows an example block of code.
    GUID-20230703-SS0I-RW53-97ZP-1X4TPF9CTSLP-low.png Figure 4-15 Initializing JESD IP in the Agilex FPGA
  21. Wait until the AFE7769D configuration completes in the TI AFE77xxD Latte software where it should report successful JESD204C link up on the AFE7769D chip in the log window (note that the 2 errors related to FPGA reset failure are expected). Figure 4-16 shows the log window displaying that the device was able to get the link up for the device's JESD RX.
    GUID-20230703-SS0I-HW13-TQVH-25CVWHXHMRRM-low.png Figure 4-16 AFE Configuration Complete Showing Link Up for the Device's JESD RX
  22. After the AFE7769D configuration is complete in the TI AFE77xxD Latte software press enter on the Arm node (Teraterm) to recalibrate the FPGA XCVRs (Rx only) to complete the JESD204C link up on FPGA. Figure 4-17 shows the link status report in the FPGA.
    GUID-20230703-SS0I-LV54-0NTH-MPDMLKVP2DFZ-low.png Figure 4-17 Completion of JESD204C Linkup With Status Report for the Link
  23. Run the ifconfig command to see the IP address for the eth0 interface. Figure 4-18 shows an example block of code.
    GUID-20230703-SS0I-V67T-DLRR-NZPW2HLGNNWM-low.png
    1. If the eth0 interface does not appear like in the image above use the ifconfig eth0 192.168.0.1 up command to bring the interface up. Then use the ifconfig eth0 192.168.0.1 netmask 255.255.255.0 command to set the IP address of the interface
    2. Then, you can use the ifconfig command to check that the interface has the IP address assigned, see Figure 4-18 as reference.
      GUID-20230703-SS0I-QLNR-VPM3-Q7C8TBMVHTF8-low.png Figure 4-18 Confirmation That the eth0 Interface has the Correct IP Address
    Figure 4-18 Eth0 Interface
  24. To be able to output signals from the TX RF ports and input signals from the RX and FB RF ports, the "Channel TDD" needs to be set for the required channels under test. This is done by going to the "RXFB-Test" page in the AFE77xxD GUI by clicking on "RXFB-Test" on the left side of the software window. In the "Channel TDD" box on this page, click on the red dots to make them green, and finally click the "Set Tdd" button; see Figure 4-20.
    GUID-20230703-SS0I-N7XD-RXSF-HQ6PZPNB3CXK-low.png Figure 4-20 TDD Configuration for TX to RX Test

    Note that when testing the FB channels, the TDD for the RX channels should not be set (such that, the dots for the RX channels are not green), see Figure 4-21.

    GUID-20230703-SS0I-CKC6-7SFW-5PXN7MJ89DMX-low.png Figure 4-21 TDD Configuration for TX to FB Test