SBOA367B December 2019 – June 2022 TLV9001 , TLV9002 , TLV9004 , TLV9051 , TLV9052 , TLV9054 , TLV9061 , TLV9062 , TLV9064
Figure 6-5 displays an amplifier circuit in the buffer configuration and its equivalent model when the amplifier is placed in the shutdown mode. Similarly to the non-inverting configuration, the input signal can pass through the differential input capacitance between the input terminals of the op amp.