SLAAE72 December 2022 MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
Current evaluation is a common requirement in low-power application, which can be used to evaluate the system running time and select the suitable power IC. There are two ways to evaluate the current.
First, use the configuration from SysConfig and estimate the current consumption. This feature will be included for MSPM0 in the future. You need to input the ADC conversion frequency, op-amp power mode, clock frequency, and so on. It outputs the following values:
Second, you can calculate the current according to the parameters in the data sheet. First, refer to the Supply Current Characteristics section in the data sheet to know the basic MCU current consumption under certain power modes. Second, refer to the specifications for all peripherals that are used to find the current consumption for each. Third, add these values together to calculate the total current consumption.