SLAAE75A November 2022 – March 2023 MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
The VBOOST circuit in the PMU generates an internal VBOOST supply which is used by the analog muxes in COMP, GPAMP, and OPA, if present on a device. The VBOOST circuit enables consistent analog mux performance across the external supply voltage (VDD) range.
SYSCTL automatically manages the enable request for the VBOOST circuit based on the following parameters:
VBOOST is disabled by default following a SYSRST. It is not necessary for application software to enable the VBOOST circuit before using the COMP, OPA, or GPAMP. When a COMP, OPA, or the GPAMP is enabled by application software, SYSCTL will also enable the VBOOST circuit to support the analog peripheral.
The VBOOST circuit has a startup time requirement (12 µs typical) to transition from a disabled state to an enabled state. In the event that the startup time of the COMP, OPA, or GPAMP is less than the VBOOST startup time, the peripheral startup time is extended to account for the VBOOST startup time.
The PMU provides a temperature and supply voltage stable bandgap voltage reference which is used by the device for internal functions, including:
The bandgap reference is enabled in RUN, SLEEP, and STOP modes. It operates in a sampled mode in STANDBY to reduce power consumption. It is disabled in SHUTDOWN mode. SYSCTL manages the bandgap state automatically; no user configuration is required.