SLAAE93 February 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
Some MSPM0G and MSPM0L devices support two OPAs. If two OPAs are available on the device, they can be used as a differential amplifier or as cascaded mode.
#FIG_UM1_HLP_VVB shows an example of how to form a differential amplifier with two OPAs in an MSPM0 device.
This circuit either adds or subtracts the voltages based on the resistors R1 and R2. The voltage difference can be calculated by the equation in the diagram, and the OPA output can also be measured by MSPM0 on board ADC or as an input to the comparator.
If the gain of one OPA is not enough, to obtain additional gain, the two OPAs can be configured as cascaded mode. #FIG_XFV_PLP_VVB shows a diagram of a cascaded amplifier. The total gain is based on the configurations of the resistors R1, R2, R3, and R4.