SLAAEB4 april 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
There are three user-configurable parameters in eeprom_emulation_type_b.h. These parameters can be configured accordingly, depending on the requirements of the application.
When only the number of groups is configured, the change can be seen in Figure 4-1. When only the sectors in one group is configured, the change can be seen in Figure 4-2. Both configuration methods will increase the Flash area used, thereby increasing the cycling capability. But when configuring the number of groups, the maximum number of data items does not change. When configuring the number of sectors in one group, the maximum number of data items will change accordingly.