SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2228 , MSPM0L2228-Q1
A generic route is a route in which the comparator peripheral publishing the event is configured to use one of several available generic route channels to publish its event to another entity (or entities, in the case of a splitter route), where an entity can be another peripheral, a generic DMA trigger event, or a generic CPU event.
The GEN_EVENT register is used to select a peripheral condition (Table 23-185) to use for publishing an event. FPUB_1 is the publisher port register and it is used to configure which generic route channel to use to broadcast the event. A second peripheral, the DMA, or the CPU can subscribe to this event by configuring its subscriber port to listen on the same generic route channel which the publishing peripheral is connected to.
For example, through the use of a generic event channel, it is possible to directly trigger a timer capture from a comparator event, by connecting a comparator FPUB_1 and TIM FSUB_x to the same generic event channel. Refer to Section 7.1.3.3 and Section 7.2.3 for how generic event route works.
IIDX STAT | Name | Description |
---|---|---|
0x01 | COMPIFG | The interrupt flags COMPIFG and COMPINVIFG are set either on the rising or falling edge of the comparator output, selected by the IES bit. When IES bit is 0, rising edge of the comparator output sets the COMPIFG and falling edge sets the COMPINVIFG. When IES bit is 1, falling edge of the comparator output sets the COMPIFG and rising edge sets the COMPINVIFG. |
0x02 | COMPINVIFG | The interrupt flags COMPIFG and COMPINVIFG are set either on the rising or falling edge of the comparator output, selected by the IES bit. When IES bit is 0, rising edge of the comparator output sets the COMPIFG and falling edge sets the COMPINVIFG. When IES bit is 1, falling edge of the comparator output sets the COMPIFG and rising edge sets the COMPINVIFG. |
0x03 | OUTRDYIFG | Comparator output ready interrupt. This bit is set when the comparator output is valid. |
See Section 7.2.5 for guidance on configuring the Event registers.