SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
To configure which peripheral interrupt source is to be used to trigger an event, set the bit which corresponds to the desired interrupt source in the IMASK register which corresponds to the desired event. Setting a bit in IMASK will cause the raw interrupt status in the RIS register to propagate to the MIS register. When an interrupt status bit in the MIS register is set (due to the interrupt being unmasked in the IMASK register and a raw interrupt being pending in the RIS register), an event is generated.
Multiple interrupt sources can be enabled for CPU interrupt events, as application software can determine the cause of the interrupt by reading the IIDX or MIS register.
For hardware events such as DMA triggers and generic event publishers, only one interrupt source should be unmasked in IMASK.