SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The ADC module provides many interrupt sources which can be configured to source the DMA trigger. In order of decreasing interrupt priority, the DMA trigger events from the ADC are given in Table 28-506. When the DMA channel is needed by the ADC, the DMA trigger should be unmasked in the IMASK register of DMA_TRIG and the DMA should be configured as needed to support the ADC operation.
Index (IIDX) | Name | Description |
---|---|---|
0x0 | NO_INTR | No bit set (IIDX.STAT = 0) means there is no pending interrupt request |
0x9 up to 0x20 | MEMRESIFG[0 up to 24](1) | Memory register interrupt flag is set when MEMRESx is loaded with a new conversion result |
The DMA trigger event configuration is managed with the DMA_TRIG event management registers. The interrupt (RIS) flags are cleared based on ACK from DMA. See Section 7.2.5 for guidance on configuring the Event registers for DMA triggers.