SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2228 , MSPM0L2228-Q1
Peripheral interrupt exceptions and system exceptions temporarily pause the processor's normal execution flow so that the processor can be used to handle an event.
The following can cause interruption of normal execution flow:
Exceptions are prioritized by the processor together with the nested vectored interrupt controller (NVIC). Each exception has either a fixed priority (reset, NMI, hard fault) or a configurable priority (SVCall, PendSV, SysTick, peripheral IRQs). Exceptions with configurable priority can be disabled by application software running in privileged mode. Exceptions with fixed priority cannot be disabled.
The processor exception model supports preemption, tail-chaining, and late-arrival features to boost exception handling performance:
An exception entry is issued if and when all of the following are true:
Processor exceptions are vectored. When an exception occurs, the current processor state is pushed onto the stack which was active at the time of the event, and execution is vectored to the entry point address in the vector table corresponding to the exception which is to be processed.
If the exception is tail-chained to a previous handler which has completed, then there is no need to push any state to the stack and the interrupt service routine can be vectored to immediately. Likewise, if the exception is higher priority than a previous exception which started entry but did not complete entry, then there is no need to save the context again (late arrival).
Upon completion of an exception handler, if there is no exception pending which needs to be handled then the processor will pop the state from the stack and restore the processor to the previous state which it was in when the exception occurred.