SLAU887 February 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
Structure
Header |
Length |
RSP |
Data |
CRC32 | ||||
---|---|---|---|---|---|---|---|---|
0x08 |
0x05 |
0x00 |
0x32 |
D1...D4 |
C1 |
C2 |
C3 |
C4 |
Description
The command returns the CRC value in response to the standalone verification command
Data
32 bit CRC value calculated for the requested memory region. D1...D4, where D1 is the least significant byte of the CRC32.