SLAU887 February 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
BSL status gives the details about any error occurred during the execution, that resulted in unresponsive BSL. This 32-bit status information is stored in a specific SRAM address (0x200000C0), and can be read through the debugger, if the debug-access is enabled in the BCR configuration.
Byte 4 |
Byte 3 |
Byte 2 |
Byte 1 |
---|---|---|---|
Reserved |
HW Error |
HW Error details |
SW Error |
Error | Description |
---|---|
0x01 | BSL Configuration CRC Error |
Error | Description | HW Error Details |
---|---|---|
0x07 | NMI exception | NMIIDX - NMI Interrupt Index register data |