SLAU887 February 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
The type of communication interface used in the Flash plug-in is configured in the BSLPLUGINCFG.PLUGINTYPE field in BSL configuration memory (see the technical reference manual in GUID-B9D85FB4-58FA-49A6-B348-0AAC807C61CF.html).
If the plug-in type has any of the ROM interface types (UART or I2C), the flash plug-in overrides the ROM implementation. If the type has a new type that is not available in ROM (for example, SPI), the plug-in is added as a new interface.
No. | Interface | Plug-in Type |
---|---|---|
1 | UART | 0x1000 |
2 | I2C | 0x2000 |
3 | Any other interface | 0xXXXX |
As shown in #FIG_MFC_2HT_NVB, after checking the flash plug-in type, the updated interface list is used for auto detection. Even after flash plug-in registration the ROM interfaces can be used if those interfaces are not overridden.