SLLA383A February 2018 – August 2022 SN65HVDA100-Q1 , SN65HVDA195-Q1 , TLIN1022-Q1 , TLIN1029-Q1 , TLIN2022-Q1 , TLIN2029-Q1 , TMS320F28P550SJ , TMS320F28P559SJ-Q1
Standby Mode is also a low-power mode, and is the mode the transceiver transitions to when a wakeup request is sent, but the EN pin is still in a low state. The main difference between Standby and Sleep mode is that in Standby mode, the RXD output is low, while in Sleep mode the RXD output is floating. This signals to the controller that the device is in Standby mode after a wakeup request, and can be transitioned into Normal Mode through the control of the EN pin. Without the EN pin held high at power up, the LIN transceiver turns on in Standby mode by default.