SLVAEQ2 April 2020 TPS2549-Q1 , TPS254900-Q1 , TPS254900A-Q1 , TPS2556-Q1 , TPS2557-Q1 , TPS2559-Q1 , TPS25830-Q1 , TPS25831-Q1 , TPS25832-Q1 , TPS25833-Q1 , TPS25840-Q1 , TPS25842-Q1
Due to the load waveform of the OCP test related to Ia, the different applications need to be sorted by current. For standard USB type-A and type-C applications, the typical current type is 1.5A, 2.1A, 2.4A and 3A. Previously, you needed to respond quickly to overcurrent by either turning off the output voltage or limiting the current. Now, to pass the MFi OCP test, the device should not shutdown the current and the voltage cannot have a big drop. In view of this situation, here are two solutions:
These two solutions are the main ideas. Sometimes, capacitors need to be added to make up the IC limitations. I will use TPS25830-Q1 EVM board to do experiments to verify the above two methods, we have set the cable compensation on the EVM board, so you can see that the output voltage has a little changes with load current in the later test result. For more information on this board, see the TPS25830-Q1 Evaluation Module User's Guide. The main points to be mentioned in this application report are shown in Figure 4.