SLYT846 February   2024 TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPS6287B10 , TPS6287B15 , TPS6287B20 , TPS6287B25 , TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15

 

  1.   1
  2. 1Introduction
  3. 2DCS-Control topology overview
  4. 3Fixed-frequency DCS-Control topology overview
  5. 4Switching frequency variation
  6. 5Lower-ripple power-save mode
  7. 6Stacking (paralleling) for higher (or lower) load currents
  8. 7Conclusion
  9. 8References

Switching frequency variation

In addition to maintaining the fast transient response, which can be further improved and tuned through the external compensation on the COMP pin, fixed-frequency DCS-Control provides a fixed switching frequency with a tight tolerance specification. Because the switching frequency is directly set with an oscillator instead of indirectly controlled with an on-timer, the frequency’s tolerance is specified in the device-specific data sheet. Table 1 and Table 2 compare the switching frequency specifications of the TPS62876-Q1, using the fixed-frequency DCS-Control topology, versus the typical frequency specification of the DCS-Control TPS62869 step-down converter.

Table 1 The TPS62876-Q1, using the fixed-frequency DCS-Control topology, specifies a ±10% tolerance of its four switching frequency options over the full temperature and input voltage ranges.
Parameter Test Conditions MIN TYP MAX Unit
fSW Switching Frequency fSW = 1.5MHz, PWM operation 1.35 1.5 1.65 MHz
fSW = 2.25MHz, PWM operation 2.025 2.25 2.475
fSW = 2.5MHz, PWM operation 2.25 2.5 2.75
fSW = 3MHz, PWM operation 2.7 3 3.3
Table 2 The TPS62869, using DCS-Control, only specifies a typical switching frequency.
Parameter Test Conditions MIN TYP MAX Unit
fSW PWM switching frequency IOUT = 1A, VOUT = 0.9V 2.4 MHz

Figure 4 and Figure 5 compare the actual variation of the switching frequency versus load current in an application. Both devices support power-save mode, which reduces the frequency at lower load currents (toward the left of both graphs). Operation in PWM mode (at higher currents) results in a precisely controlled switching frequency for fixed-frequency DCS-Control, while the switching frequency of DCS-Control increases slightly with an increasing load. In forced PWM mode (not shown), fixed-frequency DCS-Control maintains its constant frequency down to no load.

GUID-20240129-SS0I-BZHK-MHM2-WRPFX29HZLLJ-low.svg Figure 4 Switching frequency variation of the TPS62869 with DCS-Control.
GUID-20240129-SS0I-ZB7G-Z1GX-DDFRFQSH7K5M-low.svg Figure 5 Switching frequency variation of the TPSM8287A12 power module with fixed-frequency DCS-Control.

Besides power-save mode, there are two conditions where the switching frequency can deviate from the frequency set by the oscillator: during a strong load transient and if the minimum on-time is reached. When applying a heavy load, the high-side MOSFET may be on for longer than a full switching period, and when removing a heavy load, it may be off for longer than a full switching period. Both scenarios result in one or more pulses that are not present because of the extended on- or off-times.

If the minimum on-time of the high-side MOSFET is reached, both fixed-frequency DCS-Control and DCS-Control reduce the switching frequency in order to meet the minimum on-time and maintain output-voltage regulation. This is improved performance compared to some current-mode devices that maintain the frequency but let the output voltage rise in order to meet the required minimum on-time. While both fixed-frequency DCS-Control and DCS-Control reduce the switching frequency in the same way [2], fixed-frequency DCS-Control has fewer operating conditions during which the minimum on-time is reached, and the frequency reduced, because of its lower minimum on-time. For example, the TPS62876-Q1 specifies the 44ns maximum value of its minimum on-time at a 5V input voltage and across the operating temperature. Such a low value of minimum on-time enables lower output-voltage applications in automotive and aerospace and defense, for example, to operate in the higher-frequency region sometimes required by the overall system.