SPRAC76G November 2022 – February 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5726 , AM5728 , AM5729 , AM5746 , AM5748 , AM5749 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442 , AM6526 , AM6528 , AM6546 , AM6548
The PCB stack-up (or layer assignment) is an important factor in ensuring optimal performance of a power distribution scheme. An optimized PCB stack-up for improved power integrity performance can be achieved by following these recommendations:
The placement of power and ground planes in the PCB stack-up (determined by layer assignment) has a significant impact on the parasitic inductance of the power current path as shown above. For this reason, it is recommended to consider layer order in the early stages of the PCB PDN design cycle, putting high priority supplies in the top half of the stack-up and low-priority supplies in the bottom half of the stack-up as shown in the examples below. Figure 2-2 and Figure 2-3 show examples of typical PCB stack-ups designed with power distribution performance in mind. Device-specific stack-up examples can be found in Section 8.