SPRADL6 January   2025 F29H850TU , F29H859TU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F2808 , TMS320F2808-Q1 , TMS320F2809 , TMS320F2810 , TMS320F2810-Q1 , TMS320F2811 , TMS320F2811-Q1 , TMS320F2812 , TMS320F2812-Q1 , TMS320F28232 , TMS320F28232-Q1 , TMS320F28234 , TMS320F28234-Q1 , TMS320F28235 , TMS320F28235-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SJ , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Getting Started
    1. 2.1 Software Installation
      1. 2.1.1 Install Code Composer Studio IDE
      2. 2.1.2 Install C2000 IDEA Extension
    2. 2.2 Import Project
    3. 2.3 Detect Project
    4. 2.4 Basic Commands
    5. 2.5 Global Settings
      1. 2.5.1 Project-less Detection
  6. 3Overview
  7. 4Features
    1. 4.1 Targeted Collateral Delivery
      1. 4.1.1 Key Collateral
      2. 4.1.2 Additional Resources
      3. 4.1.3 Register Vision
    2. 4.2 Developer Efficiency Tools
      1. 4.2.1 Register Coder
      2. 4.2.2 Interrupt Coder
    3. 4.3 Migration Support
      1. 4.3.1 Driverlib Migration
        1. 4.3.1.1 File-Based Migration Check
        2. 4.3.1.2 Project-Based Migration Check
      2. 4.3.2 Bitfield Migration
    4. 4.4 Command List
  8. 5Summary
  9. 6References

Basic Commands

CCS and VS Code provide a powerful palette of commands that allow users to perform most, if not all, tasks using solely the keyboard. These commands can be activated using CTRL+SHIFT+P. Refer to the table below for some easy-to-use commands enabled by the C2000 IDEA extension. Alternatively, select features have UI buttons available in the C2000 IDEA Features pane that automatically run the associated commands to activate the feature.

Note: See Section 4.4 in this document for the full list of commands or search "C2000" in the command pallette.

Table 2-1 C2000-IDEA Basic Commands
Purpose Commands Devices Project Detection
Open Tool Walkthrough C2000: Help Walkthrough GEN2, GEN3, GEN4 NOT REQUIRED
Run Driverlib Register Vision C2000: Run Driverlib Register Vision on Current File GEN3, GEN4 NOT REQUIRED
Run Bitfield Register Vision C2000: Run Bitfield RegisterVision on Current File GEN3, GEN4 NOT REQUIRED
Enable Register Coder C2000: Enable Register Code Write/Read GEN3, GEN4 REQUIRED
Enable Interrupt Coder C2000: Enable Interrupt Code Templates GEN3, GEN4 REQUIRED
Enable Continuous Migration Check C2000: Enable Continuous Migration Check on Current File GEN3, GEN4 REQUIRED