SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The message handler stores the message from the CAN core shift register into the respective message object in the message RAM. Not only the data bytes, but all arbitration bits and the data length code are stored into the corresponding message object. This ensures that the data bytes stay associated to the identifier even if arbitration mask registers are used.
The NewDat bit is set to indicate that new data (not yet seen by the software) has been received. The software should reset the NewDat bit when it reads the message object. If at the time of the reception the NewDat bit was already set, MsgLst is set to indicate that the previous data (supposedly not seen by the software) is lost. If the RxIE bit is set, the IntPnd bit is set, causing the DCAN_INT to point to this message object.
The TxRqst bit of this message object is reset to prevent the transmission of a remote frame, while the requested data frame has just been received.