SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The events WAKEUPPND, RXOK, TXOK and LEC in the error and status register (DCAN_ES) belong to the status change interrupts. The status change interrupt group can be enabled by DCAN_CTL[2] SIE bit.
If SIE is set, a status change interrupt will be generated at each CAN frame, independent of bus errors or valid CAN communication, and also independent of the message RAM configuration.
Status change interrupts can only be routed to interrupt line INT0, which has to be enabled by setting DCAN_CTL[1] IE0 = 1.
Reading DCAN_ES will clear the WAKEUPPND flag. If in global power-down mode, the WAKEUPPND flag is cleared by such a read access before the DCAN module has been waken up by the system, the DCAN may re-assert the WAKEUPPND flag, and a second interrupt may occur.