SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The interface register sets control the software read and write accesses to the message RAM. There are two interface registers sets for read/write access, IF1 and IF2 and one interface register set for read access only, IF3.
Due to the structure of the message RAM, it is not possible to change single bits or bytes of a message object. Instead, always a complete message object in the message RAM is accessed. Therefore the data transfer from the IF1/IF2 registers to the message RAM requires the message handler to perform a read-modify-write cycle: First those parts of the message object that are not to be changed are read from the message RAM into the interface register set, and after the update the whole content of the interface register set is written into the message object.
After the partial write of a message object, those parts of the interface register set that are not selected in DCAN_IF1CMD/DCAN_IF2CMD, will be set to the actual contents of the selected message object.
After the partial read of a message object, those parts of the interface register set that are not selected in DCAN_IF1CMD/DCAN_IF2CMD, will be left unchanged.
By buffering the data to be transferred, the interface register sets avoid conflicts between concurrent software accesses to the message RAM and CAN message reception and transmission. A complete message object (see Section 24.10.4.11.1, Structure of Message Objects) or parts of the message object may be transferred between the message RAM and the IF1/IF2 register set (see Section 24.10.5, DCAN Register Manual) in one single transfer. This transfer, performed in parallel on all selected parts of the message object, guarantees the data consistency of the CAN message.