SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Figure 33-16 shows the procedure used when memory booting runs with non-XIP memories. The shaded procedures are specific to each memory. The ROM code searches for the image in the first four physical blocks of the memories. Other devices use only one copy of the image and the block loop runs only once.
During image shadowing , the CH is expected to be in a separate sector before the initial software.
For more information about the GPMC module, see Section 15.4, General-Purpose Memory Controller.
The following sections describe the supported device types.