SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The software may read a received message any time via the IFx interface register. The data consistency is guaranteed by the message handler state machine. Typically the software will write first 0x7F to bits [23:16] and then the number of the message object to bits [7:0] MESSAGE_NUMBER of the command register (DCAN_IF1CMD/ DCAN_IF2CMD). That combination will transfer the entire received message from the message RAM into the interface register set. Additionally, the bits NewDat and IntPnd are cleared in the message RAM (not in the interface register set). The values of these bits in the message control register (DCAN_IF1MCTL/DCAN_IF2MCTL/DCAN_IF3MCTL) always reflect the status before resetting the bits. If the message object uses masks for acceptance filtering, the arbitration bits show which of the different matching messages has been received.
The actual value of NewDat shows whether a new message has been received since last time when this message object was read. The actual value of MsgLst shows whether more than one message has been received since the last time when this message object was read. MsgLst will not be automatically reset.