SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Several message objects may be grouped to form one or more FIFO buffers. Each FIFO buffer configured to store received messages with a particular (group of) identifier(s). arbitration and mask registers of the FIFO buffer’s message objects are identical. The end of buffer (EoB) bits of all but the last of the FIFO buffer’s message objects are ‘0’; in the last one the EoB bit is ‘1.’
Received messages with identifiers matching to a FIFO buffer are stored into a message object of this FIFO buffer, starting with the message object with the lowest message number. When a message is stored into a message object of a FIFO buffer, the NewDat bit of this message object is set. By setting NewDat while EoB is ‘0’, the message object is locked for further write accesses by the message handler until the software has cleared the NewDat bit.
Messages are stored into a FIFO buffer until the last message object of this FIFO buffer is reached. If none of the preceding message objects is released by writing NewDat to ‘0,’ all further messages for this FIFO buffer will be written into the last message object of the FIFO buffer (EoB = ‘1’) and therefore overwrite previous messages in this message object.