SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The IF1 and IF2 register sets control the data transfer to and from the message object. DCAN_IF1CMD/DCAN_IF2CMD address the desired message object in the message RAM and specifies whether a complete message object or only parts should be transferred. The data transfer is initiated by writing the message number to the bits [7:0] MESSAGE_NUMBER.
When the software initiates a data transfer between the IF1/IF2 registers and message RAM, the message handler sets the [15] BUSY bit in respective DCAN_IF1CMD/DCAN_IF2CMD to 1. After the transfer has completed, the BUSY bit is set back to 0 (see Figure 24-185).