SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
SATA is not supported on the AM570x family of devices.
In the next scheme (see Figure 33-13), it is assumed that the new version of the firmware Flash Loader Host is located in the PC host. In the same way, the application loaded to device internal L3 On-chip RAM (using the peripheral boot function of the device ROM code) is called Flash Loader Second.