SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The MN-Bypass mode will be activated if REGM = 0 or 1 is loaded into the module on the rising edge of TENABLE. TINITZ also should be pulsed to enter MN-Bypass mode. The module enters a low-power mode by gating all its internal clocks (REFCLK) and powering down the internal LDO (LDOPWDN = 1) and DCO (DCOPWDN = 1). CLKDCOLDO remains gated (low) during this mode.
When the DPLLCTRL_SATA.PLL_CONFIGURATION1[20:9] PLL_REGM bit field is updated to 0x0 or 0x1, the CLKDCOLDO output clock is gated.