SWRA670A April 2020 – October 2022 CC1350 , CC1352P , CC1352R , CC2400 , CC2420 , CC2430 , CC2500 , CC2520 , CC2530 , CC2538 , CC2540 , CC2541 , CC2543 , CC2544 , CC2545 , CC2564 , CC2590 , CC2591 , CC2592 , CC2620 , CC2630 , CC2640 , CC2650 , CC2652P , CC2652R , CC2652R7 , CC2652RSIP , CC3100 , CC3120 , CC3135 , CC3135MOD , CC3200 , CC3200MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF , WL1801MOD , WL1805MOD , WL1807MOD , WL1831
The minimum Tx off-time is defined as the period where a specific transmitter should remain off after a transmission or a communication dialogue between units or a polling sequence of other units.
The minimum listening time is defined as the minimum time that the equipment listens for a received signal at or above the LBT threshold level (see Section 4.4.1.2) immediately prior to transmission to determine whether the intended channel is available for use.
An acknowledge transmission is defined as a receipt for a received message.
For automatic operated LBT devices (either software controlled or pre-programmed devices), the manufacturer should declare all the channel LBT timings for the equipment under test.
For manual operated or event dependent devices (with or without software controlled functions), the manufacturer should declare whether the transmission, once triggered, follows a pre-programmed time-out-timer, or whether the transmitter remains on until the trigger is released or the device is manually reset.
The equipment with LBT should meet the LBT timing parameter limits shown in Table 4-11.
Parameter | Limits | Notes |
---|---|---|
Minimum Tx Off-time | >25 mSec | |
Minimum Listening time (tL) | > (tF + tPS) mSec | tF = 5 mSec, tPS should be randomly varied between 0 ms and a value of 5 ms or more in equal steps of approximately 0.5 ms as the following: -If the channel is free from traffic at the beginning of the listen time, tL, and remains free throughout the fixed part of the listen time, tF, then the pseudo random part, tPS, is automatically set to zero by the equipment itself. - If the channel is occupied by traffic when the equipment either starts to listen or during the listen period, then the listen time commences from the instant that the intended channel is free. In this situation the total listen time tL should comprise tF and the pseudo random part, tPS. |
Maximum Tx ON-time for a Single Transmission | < 2 Sec | |
Maximum Tx ON-time for a Transmission dialogue or a polling sequence | < 10 Sec | In the case the time reaches the limit then the minimum Tx off-time limit should apply automatically. |