SWRA670A April 2020 – October 2022 CC1350 , CC1352P , CC1352R , CC2400 , CC2420 , CC2430 , CC2500 , CC2520 , CC2530 , CC2538 , CC2540 , CC2541 , CC2543 , CC2544 , CC2545 , CC2564 , CC2590 , CC2591 , CC2592 , CC2620 , CC2630 , CC2640 , CC2650 , CC2652P , CC2652R , CC2652R7 , CC2652RSIP , CC3100 , CC3120 , CC3135 , CC3135MOD , CC3200 , CC3200MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF , WL1801MOD , WL1805MOD , WL1807MOD , WL1831
The Nominal Center Frequency is defined as the center frequency of the Operating Channel.
The Nominal Center Frequencies (Fc) for a Nominal Channel Bandwidth of 20 MHz are defined by the following equation.
Equation 8. Fc = 5160 + (g × 20) MHz, |
where 0 ≤ g ≤ 9 or 16 ≤ g ≤ 27 and where g should be an integer.
A maximum offset of the Nominal Centre Frequency of ±200 kHz is permitted. Where the manufacturer decides to make use of this frequency offset, the manufacturer should declare the actual center frequencies used by the equipment.
The limits on actual center frequency tolerance are shown in Table 6-3.
Equipment may have simultaneous transmissions on more than one Operating Channel with a Nominal Channel Bandwidth of 20 MHz.
Channel Frequency | Limits |
---|---|
Actual Center Frequency (Fc) | < = Fc ± 20 ppm |