SWRA670A April 2020 – October 2022 CC1350 , CC1352P , CC1352R , CC2400 , CC2420 , CC2430 , CC2500 , CC2520 , CC2530 , CC2538 , CC2540 , CC2541 , CC2543 , CC2544 , CC2545 , CC2564 , CC2590 , CC2591 , CC2592 , CC2620 , CC2630 , CC2640 , CC2650 , CC2652P , CC2652R , CC2652R7 , CC2652RSIP , CC3100 , CC3120 , CC3135 , CC3135MOD , CC3200 , CC3200MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF , WL1801MOD , WL1805MOD , WL1807MOD , WL1831
A summary of the recommendation for the 2.4 GHz and 5 GHz band Short Range Devices (SRD) are provided based on the 7 June 2019 edition of CEPT ERC Recommendation 70-03. The complete document can be downloaded from this site: ERC Recommendation 70-03. Direct links to documents and other useful links from CEPT can also be found at this site: ECO Documentation Database. The CEPT ERC recommendation 70-03 for 2.4 GHz and 5 GHz frequency bands and their application are shown in Table 2-1.
Frequency band | Power EIRP (1) | Spectrum Access and Mitigation Requirements | Modulation/Maximum Occupied Bandwidth | Application / Notes | |
---|---|---|---|---|---|
1i | 2400 – 2483.5 MHz | 10mW | No requirement | Not specified | Generic use |
3b | 2400 – 2483.5 MHz | 100mW | Adequate spectrum sharing mechanism (for example, LBT and DAA) should be implemented | Not specified | For wideband modulations other than FHSS, the maximum e.i.r.p. density is limited to 10 mW/MHz |
6c | 2400 – 2483.5 MHz | 25mW | No requirement. | Not specified | Radio determination applications including equipment for detecting movement and alert. |
11c1 | 2446 – 2454 MHz | <500mW | No requirement. | Not specified | RFID Application |
11c2 | 2446 – 2454 MHz | >500mW<= 4W | ≤ 15% duty cycle FHSS techniques should be used | Not specified | RFID Application. Power levels above 500 mW are restricted to be used inside the boundaries of a building and the duty cycle of all transmissions should in this case be ≤ 15% in any 200 ms period (30 ms on /170 ms off) |
12c | 2483.5 – 2500 MHz | 10mW | LBT+AFA and ≤ 10% duty cycle. The equipment should implement a spectrum access mechanism as described in the Applicable harmonized standard or an equivalent spectrum access mechanism | 1 MHz | Medical Implants and associated peripherals applications. |
13b1 | 2483.5 – 2500 MHz | 1mW | Adequate spectrum sharing mechanisms (for example, Listen-Before- Talk and Adaptive Frequency Agility) should be implemented by the equipment and ≤ 10% duty cycle | < = 3 MHz | Medical Data acquisition applications. MBANS, indoor only within healthcare facilities. |
Ae1 | 5150 – 5350 MHz | Refer to Table 45 | Refer to Section 6.2.7 and Section 6.2.8 | Refer to Table 44 | For Wireless Access Systems including Radio Local Area Networks (WAS/RLANs). |
Ae2 | 5470 – 5725 MHz | Refer to Table 45 | Refer to Section 6.2.7 and Section 6.2.8 | Refer to Table 44 | For Wireless Access Systems including Radio Local Area Networks (WAS/RLANs). |
1j | 5725 – 5875 MHz | 25mW | No requirement | Not specified | Generic use |
2d | 5725 – 5875 MHz | 400mW | Adequate spectrum sharing mechanism (for example, DFS and DAA) should be implemented | >= 1 MHz and <= 20 MHz | Wireless Industrial Applications (WIA). Registration and /or notification may be required. APC is able to reduce the e.i.r.p to <= 25 mW |
5a | 5795– 5805 MHz | 2W / 8W | No requirement | Not specified | Transport and Traffic Telematics (TTT) applications. Individual license may be required for 8W systems |
5b | 5805– 5815 MHz | 2W / 8W | No requirement | Not specified | Transport and Traffic Telematics (TTT) applications. Individual license may be required |
The 2.4 GHz and 5 GHz bands are covered by ERC decision, which means that these are harmonized bands in most of Europe. Being a harmonized band means that the Member States should allow the putting into service and use of radio equipment if it complies with the RED when it is properly installed, maintained, and used for its intended purpose.