SWRA670A April 2020 – October 2022 CC1350 , CC1352P , CC1352R , CC2400 , CC2420 , CC2430 , CC2500 , CC2520 , CC2530 , CC2538 , CC2540 , CC2541 , CC2543 , CC2544 , CC2545 , CC2564 , CC2590 , CC2591 , CC2592 , CC2620 , CC2630 , CC2640 , CC2650 , CC2652P , CC2652R , CC2652R7 , CC2652RSIP , CC3100 , CC3120 , CC3135 , CC3135MOD , CC3200 , CC3200MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF , WL1801MOD , WL1805MOD , WL1807MOD , WL1831
Geo-location capability is a feature of the RLAN device to determine its location at installation, at reinstallation and at each power up of the equipment, with the purpose to configure itself according to the regulatory requirements applicable at the location where it operates.
The geo-location capability may be present in the equipment or in an external device (temporary) associated with the equipment operating at the same geographical location during the initial power up of the equipment. The geographical location may also be available in equipment already installed and operating at the same geographical location.
The requirement is that the geographical location determined by the equipment should not be accessible to the user.
If the equipment cannot determine the geographic location, it should operate in a mode compliant with the requirements applicable in any of the geographic locations where the equipment is intended to operate. The manufacturer should declare whether the equipment complies with the above requirement or not.