SLAAE67 December 2022 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
One of the main features of the MSPM0 platform is its scalability. Every device with the MSPM0 prefix that has the same package and pin-count is pin-to-pin compatible for drop-in replacements. This provides a high level of flexibility, as when you begin designing with a particular MCU, you can always swap it out if your MCU requirements change further on in the design phase without having to make any changes to the board. Additionally, if the next generation of your product requires more features in the MCU, you can upgrade it and just drop it on to your new board.
Now, this scalability presents a considerable amount of options. How do you pick the right one for your application? Let’s start with some basic MCU features. The main difference between MSPM0L and MSPM0G is the CPU speed:
If your application requires the MCU to be faster than 32 MHz, then an M0G device is where you want to start. The following figure and table provide a quick comparison of some of the different offerings.
Device | CPU Speed [MHz] | Flash [KB] | SRAM [KB] | Analog Level | Special Features |
---|---|---|---|---|---|
MSPM0L110x | 32 | 32, 64 | 4 | Low | |
MSPM0L130x(1) | 32 | 8, 16, 32, 64 | 2, 4 | Low | Zero-drift op-amps |
MSPM0L134x | 32 | 8, 16, 32, 64 | 2, 4 | Medium | Dual transimpedance amplifiers, zero-drift op-amps |
MSPM0G110x | 80 | 32, 64, 128 | 16, 32 | Low | |
MSPM0G150x | 80 | 32, 64, 128 | 16, 32 | High | Zero-drift op-amps |
MSPM0G310x(1) | 80 | 32, 64, 128 | 16, 32 | Low | CAN-FD, zero-drift op-amps |
MSPM0G350x(1) | 80 | 32, 64, 128 | 16, 32 | High | CAN-FD, zero-drift op-amps |
All trademarks are the property of their respective owners.
Let’s say 32 MHz is fast enough for your application. Now, how much memory do you need? M0L devices typically have less memory than M0G devices. M0L devices with expanded memory are planned, but for now the nonvolatile memory ranges from 8KB to 64KB of flash and 2KB to 4KB of SRAM. If this is within your requirements then we’re still in good shape with M0L.
Another basic specification is the GPIO count, which is driven by the pin-count of the MCU. For now, the maximum pin count for an M0L MCU is 32 pins, which allows for up to 28 GPIOs.
With the basic requirements out of the way, let’s take a look at some other features the M0L has to offer. For now, we can break this down into two subfamilies: MSPM0L110x and MSPM0L13xx. The following figure and table provide a legend for reading the complete device name in the M0L110x subfamily.
Processor Family | MSP = Mixed-signal processor |
MCU Platform | M0 = Arm® based 32-bit M0+ |
Product Family | L = 32-MHz frequency |
Device Subfamily |
110 = ADC |
Flash Memory |
5 = 32KB 6 = 64KB |
Temperature Range |
T = –40°C to 105°C S = –40°C to 125°C |
Package Type |
DYY = SOT-16 DGS20 = VSSOP-20 RGE = VQFN-24 DGS28 = VSSOP-28 RHB = VQFN-32 |
Distribution Format |
T = Small reel R = Large reel No marking = Tube or tray |
Do you need a general purpose MCU for low- to mid-end applications? MSPM0L1105 has:
Need more memory? MSPM0L1106 is the exact same except with 64KB flash.
Now let’s take a look at MSPM0L13xx. The following figure and table provide a legend for reading the complete device name in the M0L13xx subfamily.
Processor Family | MSP = Mixed-signal processor |
MCU Platform | M0 = Arm® based 32-bit M0+ |
Product Family | L = 32-MHz frequency |
Device Subfamily |
130 = ADC, 2x OPA, COMP 134 = ADC, 2x OPA (10-pA input bias current), COMP |
Flash Memory |
3 = 8KB 4 = 16KB 5 = 32KB 6 = 64KB |
Temperature Range |
T = –40°C to 105°C S = –40°C to 125°C Q =–40°C to 125°C, AEC-Q100 qualified |
Package Type |
DYY = SOT-16 DGS20 = VSSOP-20 RGE = VQFN-24 DGS28 = VSSOP-28 RHB = VQFN-32 |
Distribution Format |
T = Small reel R = Large reel No marking = Tube or tray |
This subfamily presents more analog integration, an increased temperature range, AEC-Q100 automotive qualified options, and more memory options. Let’s say your application needs some precision analog components for sensing. MSPM0L1306 provides:
MSPM0L1346 provides the same as above, but also offers support for transimpedance amplifier configurations.
The main differences between MSPM0L110x and MSPM0L13xx is that MSPM0L13xx has more integrated analog, while MSPM0L110x is more of a general-purpose MCU. However, these MCUs share a lot of the same packages and pin-counts and are pin-to-pin compatible with each other. You can begin a design with one, and then just drop in a different one later on if needed.
Now, let’s restart the MCU selection process, and say your application requires an MCU with a frequency faster than 32 MHz. In this case, you will need something from the M0G family. The M0G family was designed for applications that require a lot of computation, so it boasts higher frequency, higher memory, more advanced analog integration, and higher pin counts than the M0L family. It also has advanced timers and a math accelerator for motor control applications, and a real time clock (RTC).
It will be expanded in the future, but for now the nonvolatile memory ranges from 32 to 128KB flash, and SRAM is 16 to 32KB. For GPIOs, the pin count is up to 64 pins for now, which allows for up to 60 GPIO.
We can break M0G further down into subfamilies to take a look at some other features it has to offer: MSPM0Gx10x, and MSPM0Gx50x. The following figure and table provide a legend for reading the complete device name in the M0Gx10x subfamily:
Processor Family |
MSP = Mixed-signal processor |
MCU Platform | M0 = Arm® based 32-bit M0+ |
Product Family | G = 80-MHz frequency |
Device Subfamily |
110 = 2x ADC 310 = 2x ADC, CAN-FD |
Flash Memory |
5 = 32KB 6 = 64KB 7 = 128KB |
Temperature Range |
T = –40°C to 105°C S = –40°C to 125°C Q =–40°C to 125°C, AEC-Q100 qualified |
Package Type |
RGE = VQFN-24 DGS28 = VSSOP-28 RHB = VQFN-32 PT = LQFP-48 PM = LQFP-64 |
Distribution Format |
T = Small reel R = Large reel No marking = Tube or tray |
Do you need a general purpose MCU with a lot of memory? MSPM0G1107 has:
MSPM0G3107 has the exact same features, but with an addition of CAN-FD and automotive AEC-Q100 qualified options.
Do you need a similar MCU but with more integrated analog? A device in the M0Gx50x subfamily may fit your needs. The following figure and table provide a legend for reading the complete device name in the M0Gx50x subfamily:
Processor Family |
MSP = Mixed-signal processor |
MCU Platform | M0 = Arm® based 32-bit M0+ |
Product Family | G = 80-MHz frequency |
Device Subfamily |
150 = 2x ADC, 2x OPA, 3x COMP 350 = 2x ADC, 2x OPA, 3x COMP, CAN-FD |
Flash Memory |
5 = 32KB 6 = 64KB 7 = 128KB |
Temperature Range |
T = –40°C to 105°C S = –40°C to 125°C Q =–40°C to 125°C, AEC-Q100 qualified |
Package Type |
RGE = VQFN-24 DGS28 = VSSOP-28 RHB = VQFN-32 PT = LQFP-48 PM = LQFP-64 |
Distribution Format |
T = Small reel R = Large reel No marking = Tube or tray |
MSPM0G1507 has similar features of MSPM0G1107, but with the addition of advanced, integrated, precision analog:
MSPM0G3507 is the same as MSPM0G1507, except it includes CAN-FD and AEC-Q100 automotive qualified options.
MSPM0G3507 has:
The main differences between MSPM0Gx10x and MSPM0Gx50x is that MSPM0Gx50x has more integrated analog, while MSPM0Gx10x is more of a general-purpose MCU. However, both families have variants that support CAN-FD and have automotive AEC-Q100 qualified options. These MCUs share a lot of the same packages and pin-counts and are pin-to-pin compatible with each other as well. You can begin a design with one, and then just drop in a different one later on if needed.