SLYU067 December 2023 DRV5011 , DRV5012 , DRV5013 , DRV5013-Q1 , DRV5015 , DRV5015-Q1 , DRV5021 , DRV5021-Q1 , DRV5023 , DRV5023-Q1 , DRV5032 , DRV5033 , DRV5033-Q1 , DRV5053 , DRV5053-Q1 , DRV5055 , DRV5055-Q1 , DRV5056 , DRV5056-Q1 , DRV5057 , DRV5057-Q1 , TMAG3001 , TMAG5110 , TMAG5110-Q1 , TMAG5111 , TMAG5111-Q1 , TMAG5115 , TMAG5123 , TMAG5123-Q1 , TMAG5124 , TMAG5124-Q1 , TMAG5131-Q1 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5231 , TMAG5253 , TMAG5273 , TMAG6180-Q1 , TMAG6181-Q1 , TMCS1107 , TMCS1108
my.TI™, E2E™, and TI.com™ are trademarks of Texas Instruments.
Webench® is a registered trademark of Texas Instruments.
All trademarks are the property of their respective owners.
Magnetic sensors use technologies, such as the Hall-effect or magneto-resistive structures, to determine the magnitude or direction of an externally supplied magnetic field. These sensors detect the motion and position of key elements within a system by measuring the behavior of the field surrounding a permanent magnet. The device can track and define operating positions that help create user-friendly features, safety functions, and improve system monitoring and reliability.
The key challenge in designing with these sensors is that magnetic fields are invisible and not innately intuitive. As a result, designing many functions without the aid of a simulation tool can be difficult. Texas Instruments' Magnetic Sense Simulator (TIMSS) is available to use for free at Webench® on TI's website. This tool is a replacement to the Magnetic Sense Enhanced Proximity Tool. Related documentation and information is accessible at TI Magnetic Sense Simulator in the tool folder.
This software was built around Python libraries that enable quick approximations using an equation-based solver. This approach is somewhat limited because the tool only supports a single magnetic body and does not include the option to simulate the interaction with nearby ferromagnetic materials. More advanced tools that use a finite element method where systems are solved using complex 3D meshes are typically capable of supporting such efforts but these are often time consuming and require significant tools training to reach proficiency.
The purpose of TIMSS is to provide a platform which can parametize common types of motion to enable fast simulations and approximate device behavior under various conditions. The tool allows for control of temperature and parametric sweeps to evaluate system response across multiple tolerances. This evaluation is particularly helpful before attempting to prototype or run advanced simulations which involves significant computing time.
To aid the user with design development, TIMSS stores saved designs. Support of this functionality requires a myTI.com account. Please refer to the following links for help with setting up a my.TI™ on-line information services account.
The purpose of this guide is to explain the features and functions of Texas Instruments' Magnetic Sense Simulator (TIMSS) and to explain methods and approaches that aid in successful simulation configurations.
For questions about using TIMSS, please reach out on E2E™ support.
There are four basic types of motion defined within Texas Instruments' Magnetic Sense Simulator (TIMSS). These definitions have a certain degree of flexibility in each that allows for quick customization of the simulation environment. The types of motion supported are:
Up to six sensors can be placed simultaneously in each of these formats to evaluate relative placement and response as a system. The magnet and sensor can be rotated to match the user system configuration in all cases. Furthermore, plots relative to the sensor alignment provide the observed magnetic field and the sensor output.
A library of magnetic materials and predefined shapes are included in TIMSS and allows for a highly customizable magnetic source, which allows for both standard dipole magnets or more complex multipole structures.
Static position calculations are also available in TIMSS to quickly determine if the field produced by a magnetic structure is strong enough or in the correct direction to be useful in a given application.