CC256XC-BT-SP

CC256xC 向け Bluetooth® サービス・パック

CC256XC-BT-SP

ダウンロード

概要

The CC256xC Bluetooth Service Pack (SP) contains the mandatory initialization scripts (BTS files) that have platform specific configurations and bug fixes.

In addition, the Bluetooth Service Pack also contains companion files for the CC2564C device that are useful for testing and debugging. The Service Pack is composed of the following files:

  • Init Script BTS file (initscripts-TIInit_6.12.26.bts)
  • Init Script Add-ons
    • Audio/Voice processing add-on (initscripts-TIInit_6.12.26_avpr_add-on.bts)
    • BLE add-on (initscripts-TIInit_6.12.26.ble_add-on.bts)
  • ILI file (TIInit_6.12.26.ili)
  • XML file (TIInit_6.12.26.xml)
  • License Agreement
  • Readme / Release Notes

Note: The version in the file name is unique for combination of hardware and firmware, but is not updated per release. The version information is updated within the files. 

Please start by reading the license agreement and readme file. The service pack files are described below.

  • BTS file
    • BTS is an abbreviation for Bluetooth script. The BTS file is a binary file that contains HCI commands and actions for the Texas Instruments Bluetooth Devices. HCI interface is bi-directional. For each HCI command sent from the host to the Bluetooth controller, the Bluetooth controller responds with an HCI Event. In order to simplify the format and procedures required to successfully execute these HCI commands, the BTS format is used. BTS files are distributed under Texas Instruments license. See the accompanying license file for more details.
    • BTS functionality
      • The primary usage of the BTS is to trigger the initialization sequence after the Bluetooth device powers up. The initialization script must be executed after every device power-up. BTS initialization scripts contain a section of memory write commands (written code to RAM) that perform as a software patch to fix potential ROM issues of the Bluetooth device. Although this is not the primary purpose of the BTS format, it can also be used in any scenario to load HCI commands to the Bluetooth device. BTS files may also be used for platform-related commands such as to enable deep-sleep mechanism, changing UART baud rate, audio configurations, etc. The BTS file is device specific and will only operate on the CC256xC devices listed below. The latest Bluetooth service pack for a CC256xB device can be found in the following link: [https://www.ti.com/tool/CC256XB-BT-SP].
  • ILI file
    • The ILI file decodes Bluetooth firmware logger messages in a readable format. It is used by the logger tool included in the Wireless Tools software package.
  • XML file
    • The XML file describes the vendor specific HCI commands, events and their parameters. It is used by the HCITester and logger utilities included in the Wireless Tools software package.
特長
  • Classic Bluetooth and Bluetooth Low Energy
  • Sleep Enabled

ダウンロード

技術資料

結果が見つかりませんでした。検索条件をクリアしてから、再度検索を試してください。
15 をすべて表示
種類 タイトル 最新の英語版をダウンロード 日付
その他の技術資料 TI Engineering Evaluation Units vs. MIL-PRF-38535 QML Class V Processing (Rev. A) 2023/08/31
アプリケーション・ノート Heavy Ion Orbital Environment Single-Event Effects Estimations (Rev. A) PDF | HTML 2022/11/17
アプリケーション・ノート Single-Event Effects Confidence Interval Calculations (Rev. A) PDF | HTML 2022/10/19
サイバー セキュリティ報告書 Bluetooth® Classic – BrakTooth V12 vulnerability 2021/12/21
ユーザー・ガイド CC2564C TI Dual-mode Bluetooth Stack on MSP432 MCUs (Rev. B) PDF | HTML 2021/12/20
ユーザー・ガイド CC2564C TI Dual-mode Bluetooth Stack on STM32F4 MCUs (Rev. B) PDF | HTML 2021/12/02
サイバー セキュリティ報告書 InjectaBLE: Injecting Malicious Traffic Into Established Bluetooth® Low Energy 2021/06/22
サイバー セキュリティ報告書 Bluetooth® SIG Erratum – Impersonation in the Passkey Entry Protocol (Rev. A) 2021/05/27
サイバー セキュリティ報告書 Bluetooth® SIG Erratum – Authentication of the LE Legacy Pairing Protocol (Rev. A) 2021/05/27
サイバー セキュリティ報告書 Bluetooth® Low Energy, Basic/Enhanced Data Rate–PIN-Code Pairing Key Derivation 2021/05/27
データシート CC2564C Dual-Mode Bluetooth® Controller データシート (Rev. B) 2020/12/02
サイバー セキュリティ報告書 Bluetooth Low Energy – Invalid Connection Request (SweynTooth) (Rev. A) PDF | HTML 2020/07/17
サイバー セキュリティ報告書 Bluetooth Low Energy, Basic Rate/Enhanced Data Rate – Method Confusion Pairing V PDF | HTML 2020/05/18
サイバー セキュリティ報告書 Bluetooth Basic Rate/Enhanced Data Rate – Bluetooth Impersonation AttackS (BIAS) PDF | HTML 2020/05/18
その他の技術資料 HCITester Tool (Rev. B) 2015/09/16

関連する設計リソース

ソフトウェア開発

アプリケーション・ソフトウェアとフレームワーク
WILINK-BT_WIFI-WIRELESS_TOOLS WL18XX モジュール向け、WiLink™ ワイヤレス・ツール
ドライバまたはライブラリ
CC2564CMSP432BTBLESW MSP432 MCU 向け CC2564C TI デュアルモード Bluetooth® スタック CC2564CSTBTBLESW STM32F4 MCU 向け CC2564C TI デュアルモード Bluetooth® スタック TI-BT-4-2-STACK-LINUX-ADDON Linux プラットフォーム向け、WL183x と CC2564C 搭載 TI Bluetooth 4.2 スタック・アドオン
ソフトウェア開発キット (SDK)
TIBLUETOOTHSTACK-SDK Stonestreet One Bluetopia に基づく TI Bluetooth スタック

サポートとトレーニング

TI E2E™ フォーラムでは、TI のエンジニアからの技術サポートを提供

投稿されたすべてのフォーラムトピック (英語) を表示

コンテンツは、TI 投稿者やコミュニティ投稿者によって「現状のまま」提供されるもので、TI による仕様の追加を意図するものではありません。使用条件をご確認ください。

TI 製品の品質、パッケージ、ご注文に関するお問い合わせは、TI サポートをご覧ください。