SLVSHH4 July 2024 TPS546E25
ADVANCE INFORMATION
The Supported PMBus Commands and Default Values Table lists the implemented registers and also the default for the bit behavior and register values.
Command Code | Command Name | R/W | NVM | Default Value (Hex) | Default Behavior |
---|---|---|---|---|---|
01h | OPERATION | R/W | NO | 04h | Defines the operation of the device. |
02h | ON_OFF_CONFIG | R/W | YES | 16h | Turn ON/OFF by CNTL pin, Use TOFF_DELAY |
03h | CLEAR_FAULTS | W | NO | N/A | Clear all faults. |
04h | PHASE | R | NO | N/A | STACK_POSITION set by pinstrap selection. |
09h | P2_PLUS_WRITE | W | NO | N/A | Page Plus Write function to send a command to a specific page and phase or all phases. |
0Ah | P2_PLUS_READ | R/W | NO | N/A | Page Plus Read function to read data in a specific page and phase or all phases. |
0Eh | PASSKEY | R/W | YES | 00h | Passkey to lock access to (DDh) EXT_WRITE_PROTECTION |
10h | WRITE_PROTECT | R/W | YES | 00h | All commands are writable. |
15h | STORE_USER_ALL | W | NO | N/A | Stores all current storable register settings into NVM. |
16h | RESTORE_USER_ALL | W | NO | N/A | Restores all storable register settings from NVM. |
19h | CAPABILITY | R | NO | D0h | The device has an SMB_ALERT# pin. |
1Bh | SMBALERT_MASK | R/W | YES | N/A | Sets ability to mask events that trigger SMB_ALERT#. |
20h | VOUT_MODE | R | NO | 97h | Indicates the device is relative format with an exponent value of -9 for an equivalent LSB of 1.953mV. |
21h | VOUT_COMMAND | R/W | NO | VBOOT | Set the output voltage through PMBus. |
22h | VOUT_TRIM | R/W | YES | 0000h | Apply a fixed offset voltage to the output voltage command value. |
24h | VOUT_MAX | R/W | YES | VSEL | Maximum output voltage, initially set by pinstrap and settable by PMBus. |
25h | VOUT_MARGIN_HIGH | R/W | YES | 0210h | Sets the margin high percentage when selected in OPERATION register. |
26h | VOUT_MARGIN_LOW | R/W | YES | 01F0h | Sets the margin low percentage when selected in OPERATION register. |
27h | VOUT_TRANSITION_RATE | R/W | YES | E850h | Sets the rate in mV/μs the output changes voltage. |
29h | VOUT_SCALE_LOOP | R/W | YES | E804h | Sets the feedback resistor ratio. |
2Ah | VOUT_SCALE_MONITOR | R/W | YES | E804h | Sets the feedback resistor ratio when external feedback divider is used for telemetry purposes. |
2Bh | VOUT_MIN | R/W | YES | 80h | Minimum output voltage, initially set by pinstrap and settable by PMBus. |
33h | FREQUENCY_SWITCH | R/W | YES | 3806h | Sets the switching frequency with default set to 800kHz. |
35h | VIN_ON | R/W | YES | 0002h | PVIN ON threshold, 2.5V |
36h | VIN_OFF | R/W | YES | 0002h | PVIN OFF threshold, 2.3V |
39h | IOUT_CAL_OFFSET | R/W | YES | F000h | Used to add or subtract a fixed offset from READ_IOUT with default of 0A. |
40h | VOUT_OV_FAULT_LIMIT | R/W | YES | 024Dh | VOUT Tracking OV Fault threshold = +12% |
41h | VOUT_OV_FAULT_RESPONSE | R/W | YES | RESPONSE | Fault Response to OV, Set by Pin Detect or override through PMBus |
42h | VOUT_OV_WARN_LIMIT | R/W | YES | 0233h | VOUT Tracking OV Warning threshold = +8% |
43h | VOUT_UV_WARN_LIMIT | R/W | YES | 01CDh | VOUT Tracking UV Warning threshold = −8% |
44h | VOUT_UV_FAULT_LIMIT | R/W | YES | 01B3h | VOUT Tracking UV Fault threshold = −24% |
45h | VOUT_UV_FAULT_RESPONSE | R/W | YES | RESPONSE | Fault Response to UV, Set by Pin Detect or override through PMBus |
46h | IOUT_OC_FAULT_LIMIT | R/W | YES | IOCL | Low-side valley current limiting threshold, Set by pinstrap or NVM if pinstrap override is cleared. |
48h | IOUT_OC_LV_FAULT_LIMIT | R | NO | 01B3h | Same contents as VOUT_UV_FAULT_LIMIT |
49h | IOUT_OC_LV_FAULT_RESPONSE | R | NO | RESPONSE | Same contents as VOUT_UV_FAULT_RESPONSE |
4Ah | IOUT_OC_WARN_LIMIT | R/W | YES | 0032h | Programmable Overcurrent warn limit, 50A |
4Fh | OT_FAULT_LIMIT | R/W | YES | 1022h | Programmable OT Fault threshold = 145 °C |
50h | OT_FAULT_RESPONSE | R/W | YES | RESPONSE | Fault Response to OT, Set by Pin Detect or override through PMBus |
51h | OT_WARN_LIMIT | R/W | YES | 1022h | Programmable OT Warning threshold = 125 °C |
55h | VIN_OV_FAULT_LIMIT | R/W | YES | 809h | PVIN OV Fault threshold = 18.5V |
60h | TON_DELAY | R/W | YES | F800h | 50μs delay when a start condition is received (as programmed by the ON_OFF_CONFIG register) until the output voltage starts to rise |
61h | TON_RISE | R/W | YES | F800h | 0.5ms from when the output starts to rise until the output voltage has entered the regulation band |
64h | TOFF_DELAY | R/W | YES | F800h | 0ms from when a stop condition is received (as programmed by the ON_OFF_CONFIG register) until the unit starts the soft-stop operation |
65h | TOFF_FALL | R/W | YES | F800h | 0.5ms from the end of the turn-off delay time until the internal reference DAC is commanded to 0mV |
78h | STATUS_BYTE | R | NO | 41h | Status is device is OFF, and OTH is 1b. |
79h | STATUS_WORD | R | NO | 2841h | VIN is off and PGOOD_Z is 1b. |
7Ah | STATUS_VOUT | R/W | YES | 0h | Current status |
7Bh | STATUS_IOUT | R/W | YES | 0h | Current status |
7Ch | STATUS_INPUT | R/W | YES | 0h | Current status |
7Dh | STATUS_TEMPERATURE | R/W | YES | 0h | Current status |
7Eh | STATUS_CML | R/W | NO | 0h | Current status |
7Fh | STATUS_OTHER | R/W | NO | 0h | Current status |
80h | STATUS_MFR_SPECIFIC | R/W | YES | 0h | Current status |
88h | READ_VIN | R | NO | N/A | Measured input voltage. |
8Bh | READ_VOUT | R | NO | N/A | Measured output voltage. |
8Ch | READ_IOUT | R | NO | N/A | Measured output current. |
8Dh | READ_TEMP_1 | R | NO | N/A | Measured Controller die temperature |
98h | PMBUS_REVISION | R | NO | 55h | PMBus 1.5 |
99h | MFR_ID | R | NO | 4954h | ASCII for "TI" |
9Ah | MFR_MODEL | R | NO | 00h | Device model |
9Bh | MFR_REVISION | R/W | YES | 00h | Device revision |
ADh | IC_DEVICE_ID | R | NO | IC part number | |
AEh | IC_DEVICE_REV | R | NO | 00h | IC revision |
D1h | SYS_CFG_USER1 | R/W | YES | 0000h | |
D3h | PMBUS_ADDR | R/W | YES | N/A | Set by pinstrap, can be written through PMBus. |
D4h | COMP | R/W | YES | N/A | Set by pinstrap, can be written through PMBus. |
D5h | VBOOT_OFFSET_1 | R/W | YES | N/A | Set by pinstrap, can be written through PMBus. When external divider is selected, VBOOT is the reference voltage at the FB pin. |
D6h | STACK_CONFIG | R/W | YES | N/A | Set by pinstrap, can be written through PMBus. |
D8h | PIN_DETECT_OVERRIDE | R/W | YES | 0C7Dh | Pinstrap is used by default. |
D9h | NVM_CHECKSUM | R | NO | TBD | NVM Checksum excluding Passkey |
DAh | READ_TELEMETRY | R | NO | N/A | Read VOUT, IOUT, and TEMP with a block read. |
DBh | STATUS_ALL | R | NO | N/A | Read all STATUS with a block read. |
DDh | EXT_WRITE_PROTECTION | RW | YES | 0000h | No registers are prohibited from being written. |
DEh | IMON_CAL | R/W | YES | 07h | No gain trim for IOUT_READ |
FCh | FUSION_ID0 | R | NO | 02C0h | Device Identification used by FUSION |
FDh | FUSION_ID1 | R | NO | 4B434F4Ch | Device Identification used by FUSION |