SLUAAL1 June 2022 UCD90120A , UCD90124A , UCD90160 , UCD90160A , UCD90320 , UCD90320U , UCD9090 , UCD9090A
This section is to demonstrate how to configure a GPIO pin(FPWM2_GPIO6) to be a Hi-Z signal as shown in Figure 4-1.
The Pid ID of the FPWM2_GPIO6 is 1 from Table 3-1 and Table 3-2.
Application need send out the following commands:
Write GPIO_SELECT command to choose the target GPIO. Payload 0x01 is to select FPWM2_GPIO6 pin.
Write GPIO_CONFIG command to output HIGH signal. Payload 0x1 is to enable the Pin without output disable.