SLUAAL1 June 2022 UCD90120A , UCD90124A , UCD90160 , UCD90160A , UCD90320 , UCD90320U , UCD9090 , UCD9090A
The UCD90xxx family of digital sequencers, also known as system health monitors, are flexible and powerful enough to meet user sequencing, monitoring, margining and other needs. The entire families of devices are designed to have similar behaviors, but with a different number of rails or some other minor features. Users only need to learn how to use the device once, and can then seamlessly switch to other devices within the family that best fit their future designs. This document is to help applications to access GPIOs from the devices. This document does not apply to the UCD9080 and UCD9081 devices. All commands listed in the document can be found in the publications listed in Section 5.
All byte values are represented in hexadecimal format. These are the codes to understand all I2C communications that occur: