SLVAF66 June 2021 DRV3255-Q1 , DRV8300 , DRV8301 , DRV8302 , DRV8303 , DRV8304 , DRV8305 , DRV8305-Q1 , DRV8306 , DRV8307 , DRV8308 , DRV8320 , DRV8320R , DRV8323 , DRV8323R , DRV8340-Q1 , DRV8343-Q1 , DRV8350 , DRV8350F , DRV8350R , DRV8353 , DRV8353F , DRV8353R
At first glance in Figure 4-4, high-side drain to low-side source capacitors seem to be self-explanatory and are often confused with the decoupling or bulk capacitors. However, most motor driver applications do not have the low-side source connected to GND. Instead, the low-side source is usually connected to a shunt resistor which is used for current sensing, and is then is then connected to GND.
This is important because decoupling capacitors need stable references to reliably provide charge. GND instability can be present in a system as a result of inductance introduced by the sense resistor layout, motor current flowing through the low-side FET, or bad grounding techniques. If GND bounces along with the switch node then the decoupling capacitors cannot do their job to provide charge from a stable reference and low inductive path. For reference, a 0.2512 component package size, which is a common package for sense resistors, introduces 1–5 nH of parasitic inductance.
The HS drain to low-side source capacitor can circumvent these problems because it is connected to VDRAIN, which is assumed to be stable, and can dump charge directly onto the node, instead of through the path of a sense resistor. This is the concept of an AC GND and is the reason why the RC snubber can also be connected to the HS drain, as well as the LS source.
As a result:
A lot of engineers underestimate this mitigation technique and fail to use footprints as they have already prioritized RC snubbers and bulk capacitors at this point. If GND or the sense resistor is ringing negative, or below GND, the HS drain to LS source capacitor provides charge in a low impedance path. Waveforms showing the GND and LS source voltage are helpful to determine if negative ringing is occurring and whether to update the design to add HS drain to LS source capacitors to the half bridges.