SLVAF66 June 2021 DRV3255-Q1 , DRV8300 , DRV8301 , DRV8302 , DRV8303 , DRV8304 , DRV8305 , DRV8305-Q1 , DRV8306 , DRV8307 , DRV8308 , DRV8320 , DRV8320R , DRV8323 , DRV8323R , DRV8340-Q1 , DRV8343-Q1 , DRV8350 , DRV8350F , DRV8350R , DRV8353 , DRV8353F , DRV8353R
Plenty of theory and simulation supporting evidence for this section is found in the Understanding and Mitigating Motor Driver Board Parasitics through Simulation article. It is highly recommended to supplement the theory discussed here with the article.
Many of the sections discuss the theory but are summarized with bullet points. It is encouraged to read the section and refer back to the bullet points as a section summary.
As we progress through the section, more circuits are developed that can be added to the system. These additions might conflict with system considerations and goals, such as the need to be handheld which limits board space. Deciding what to add and what not to add is part of the art of high-power design.